Connected Fire Container Monitoring

Connected Fire

Through a culmination of years of research and development by Johnson Controls industry-leading engineers and data scientists; we bring to you Connected Fire Container Monitoring, which has been designed with agility, flexibility and scalability in mind, to enable your building to manage its operations systematically, by delivering buildings that have memory, intelligence, and unique identity.

Container Monitoring

Johnson Controls has developed the Connected Fire Container Monitoring system which has been designed to remotely monitor the pressure and temperature of our Halocarbon and Inert gas Fire Suppression Systems.

The Container Monitoring device works by collecting data from each container at set time intervals and is capable of connecting to a mobile device such as a smart phone or tablet, enabling real time data to be shared via an online dashboard.

This data can then be sent wirelessly to the cloud and analyzed to regulate the pressure based on the temperature and provide information that allows instant intervention to be taken, in the case of an unexpected change in pressure as needed to ensure the continued health of the Fire Suppression System.

Connected Fire Container Monitoring Brochure

Learn more about how the system works.
Download our Brochure

Register/Login

Access to the Container Monitoring system is granted on a company basis and will be given to a designated User Administrator. The User Administrator is then able to provide access to other users in the company and can manage their access going forward.

Access will be granted to Johnson Controls Authorized Distributors on completion of the required training, please contact your local Territory Manager PRIOR to registration.

Please follow these steps to request access:

  1. Assign one person from your company that will be the User Administrator (an additional user administrator can be added)
  2. Request company access and administrator access by Clicking Here.
  3. Johnson Controls will review your access
  4. Once approved you will receive an email with your user name and password
  5. Log into the Container Monitoring by Clicking Here.

(Container Monitoring system dashboard can then be accessed, once the request is approved).

How to download the app

Once you have received your logins you will also be able to view the dashboard through the Johnson Controls mobile app.

Download here

Alternatively, go to the Apple app store and search on Connected Fire Container Monitoring.

  1. Who can get access to Container Monitoring?

    Any customer that has received Container Monitoring training and is now an authorised distributor of this product, can have access to the dashboard by completing the registration form by Clicking Here

  2. How does the Container Monitoring system access the cloud?

    The Container Monitoring system uses an internet gateway device that can connect to the users LAN or cellular connection.

  3. How secure is the Container Monitoring System

    The Container Monitoring system uses an elelectronic gauge that is LoRaWAN 1.0.2 compliant, Class A. LoRaWAN security implements end-to-end encryption. Each LoRaWAN device is personalized with a unique 128 bit AES(1) key and a globally unique identifier (EUI-64-based DevEUI), both of which are used during the device authentication process.

  4. How does the Electronic Gauge communicate with the gateway?

    The Electronic Gauge uses the LoRa technology to communicate wirelessly with the gateway.

  1. How does the system handle low pressure alarms that may be caused by low temperature?

    The Container Monitoring system measures both the temperature and pressure and normalizes the pressure based on the actual temperature.

  2. How does this help?

    By normalizing the pressure based on the temperature, we eliminate any signals that could have been interpreted as low pressure caused by a leak.

  3. Can the Container Monitoring system be fitted to existing systems?

    Yes, the majority of JCI systems can be retrofitted with Container Monitoring.

  4. How accurate is the Container Monitoring system?

    The system is extremely accurate, capable of measuring the pressure to an accuracy of 0.5%, which will allow the detection of micro-leaks.

Available Brands

ANSUL
Hygood

Please contact your sales representative for any further questions on the Container Monitoring system. Technical contacts are provided on the contacts/support information once you have logged into the Container Monitoring dashboard.